4/10/2024 6:10 PM | |
Joined: 4/10/2024 Last visit: 4/15/2024 Posts: 1 Rating: (0) |
Hello, I want to configure Switch VLAN Interfaces (SVI) for three VLANs (10,800,900). I have created the VLANs and assigned three trunk ports lm1(4-6). In those ports will be connected switches with tagged port configuration as well. I have not found a reliable way to know if the SVI works properly. It is supposed to be configured with an IPv4 address as a gateway for each SVI. Furthermore, the routing table appears to be fine, however, the gateway of any SVI is not reachable from my PC. My PC is connected to an access port of the SW1 connected to the firewall rx1500. What could be wrong? I have checked the firewall rules but there were no entries. Any kind of example configuration, cli commands or similar would be extremely useful. I have been stuck in this configuration for days. I will attach the running-config for further reference MODEL: RUGGEDCOM RX1500: 6GK6015-0AM2 Firmware: ROX 2.16.1 Thanks for your help Regards AttachmentRX1500_runconfig_10-04-2023.txt (211 Downloads) |
Follow us on