6/11/2024 2:31 PM | |
Joined: 2/20/2014 Last visit: 8/18/2024 Posts: 396 Rating: (38) |
Hi, I am having this issue where the message "Online: Function not implemented in loaded communication driver" is displayed when I try Online access > update accessible devices via the LAN Network card in. In this adding the first attachment. AttachmentScreenshots.zip (100 Downloads) |
Last edited by: Jen_Moderator at: 06/12/2024 09:04:15All files added as .zip file. |
|
6/14/2024 4:45 AM | |
Joined: 3/11/2019 Last visit: 8/19/2024 Posts: 1555 Rating: (281)
|
Hi, looks like there is an issue with the communication drivers, at least it would be logical. But you do also use an outdated version of V16. At first I recommend to update V16 to the latest version available. Most of the time, those updates does also include improved communication drivers. Its worth a try. Updates for STEP 7 V16, S7-PLCSIM V16 and WinCC V16regards sancruz |
Feedback appreciated, please rate |
|
Follow us on