8/4/2016 12:33 PM | |
Joined: 5/12/2006 Last visit: 10/22/2024 Posts: 22431 Rating: (3028) |
Hi, can you provide the NTP Settings for Both Interfaces? Regards Christoph |
8/5/2016 5:14 AM | |
Posts: 2 Rating: (0) |
Figure PNIO settings and NTP settings. If one rack modify NTP settings on the PN-IO-X5, then they become the same PN-IO-X8. |
8/15/2016 2:30 PM | |
Joined: 4/8/2013 Last visit: 6/30/2024 Posts: 95 Rating: (7) |
We have the same problem, did you find a solution to configure NTP on the internal PNIO ports of a H system with 410's? |
Follow us on