7/6/2024 1:16 PM | |
Joined: 12/18/2014 Last visit: 8/18/2024 Posts: 33578 Rating: (4173)
|
I use various SD cards from different manufacturers and with different classes and different storage capacities (2 GB to 64 GB) for my LOGO!s. I have never had any problems. However, with the 64 GB card I had to create a 32 GB FAT32 partition because the LOGO can only read up to 32 GB. All cards formatted FAT32.
|
7/7/2024 6:33 PM | |
Joined: 4/3/2017 Last visit: 7/14/2024 Posts: 7 Rating: (1) |
My experience with logo8 and microsd has been sketchy. Not as reliable as an industrial device should be. The microsd is a maxell microsd hc class 10 16gb. I tried it formatted as FAT32 with allocated sizes ranging from 4032 to the 32kb ... the logo as soon as I insert it in diagnostics says microsd ok but when loading a program then diagnostics throws the error. In my pc I can deploy the LWE program to SD no problem, I tried writing a huge file and it records and play back with no issues. Its a compatibility between the logo and that specific card. I bought another one this time a 32 gig u1. That one worked. For me it seems it is a logo issue that needs to be adressed since lower class sd cards are harder to get. I want to know is someone can tell me how to get a error buffer or log from the logo to check why it cant write to sd card. Cheers! |
7/7/2024 6:43 PM | |
Joined: 12/18/2014 Last visit: 8/18/2024 Posts: 33578 Rating: (4173)
|
Sorry, but I can't nothing other as I wrote. But you can ask Siemens directly via Support Request. |
7/14/2024 10:47 PM | |
Joined: 4/3/2017 Last visit: 7/14/2024 Posts: 7 Rating: (1) |
Thanks. Will do. There is something strange going on on my LOGO. |
Follow us on