7/2/2024 8:31 PM | |
Joined: 7/2/2024 Last visit: 7/3/2024 Posts: 2 Rating: (0) |
Hello, Just a quick question to be sure. I already found a compatibility list but I'm not really sure. At the moment I have four 6ed1055-1nb10-0ba2 expansion modules and two 6ED1052-1MD00-0BA8 base modules. I want to replace the base modules with the new Logo 8 (8.4) for instance with the 6ED1052-1MD08-0BA2 or without LCD screen 6ED1052-2MD08-0BA2. Are these compatible with my expansion modules? I found a list but it's contradicting a little bit (the two last points) https://support.industry.siemens.com/cs/document/24931144/compatibility-overview-of-logo!-basic-and-logo!-expansion-modules-?dti=0&lc=en-BO
Thanks in advance |
7/3/2024 4:49 PM | |
Joined: 12/18/2014 Last visit: 7/18/2024 Posts: 33369 Rating: (4138)
|
It's corrected. Compatibility overview of LOGO! Basic and LOGO! Expansion modules. |
This contribution was helpful to1 thankful Users |
Follow us on