8/12/2024 12:28 PM | |
Joined: 6/30/2014 Last visit: 8/28/2024 Posts: 463 Rating: (89)
|
Dear Vikash, Nice to see you here again. I have never seen that error before, I also do not know yet a solution for it. Maybe you can create a log file of the issue, to have a look into it, maybe you can find some useful information for your troubleshooting? https://support.industry.siemens.com/cs/ww/en/view/109743938 Maybe you have a backup of the database, to do a roll back? Do you still know what has been done with the DB? In case you are sure that this is a bad behavior of COMOS itself, you may open a ticket at their support. It would be interesting to find out, maybe you can test it, if this issue only happens with your DB or also with a standard iDB which comes with the COMOS fullversion. They will proably ask how to rebuild this issue, so that the developers can debug it. All the very best, SuperPippo |
Last edited by: Moderator_Lan at: 08/12/2024 12:38:08link optimized |
|
This contribution was helpful to1 thankful Users |
Follow us on