9/25/2024 10:59 AM | |
Joined: 3/12/2024 Last visit: 10/2/2024 Posts: 48 Rating: (0)
|
Hey gera98eleven, Yes - I would highly recommend you to use an UART-cable to get connected to your IOT2050. Normally you should get the following outputs from the UART-connection:
You can find the correct connection parameters for UART in the image below (COM port may be different). Then power on your IOT2050 with the UART-connection and press any key as soon as the message "Hit any key to stop autoboot" appears. In the u-boot shell (only accessible via UART!) you can use the following commands to adjust the boot-order:
Choose the order thats best for you (mmc0 = SD card; mmc1 = eMMc) If your OS is broken you should use the Service Stick to install an image on the eMMC. You can find the image (V3.2.3) on our Downloads Page. Depending on your boot order you can manually boot from the USB1-slot from the u-boot-shell with the command:
Now you can install the IOT2050 Industrial OS image from the stick. BR |
Follow us on