3/7/2025 6:45 PM | |
Joined: 5/7/2022 Last visit: 3/31/2025 Posts: 32 Rating:
|
hello guys the image attached is a real project uploaded my question is , why the telegram start address and end address is not written |
3/10/2025 8:51 AM | |
Joined: 5/12/2006 Last visit: 4/8/2025 Posts: 22609 Rating:
|
Because this adress is not Part of the drive configuration |
3/20/2025 5:48 AM | |
Joined: 5/7/2022 Last visit: 3/31/2025 Posts: 32 Rating:
|
ok but in another control units why i can see the the telegram adress for each component and how the control unit can direct the profibus message if the telegram adress is not configured ? |
3/20/2025 6:01 AM | |
Joined: 5/12/2006 Last visit: 4/8/2025 Posts: 22609 Rating:
|
Telegram adresses are part of the PLC Data please open HW Config of the project and check that the control unit is correct assigned to a plc and check on the PLC that the adresses are rigth configured |
We are working on a new user interface with better overview and more relevance.
Follow us on