2/16/2007 9:49 AM | |
Posts: 661 Rating:
|
Hello coollogo, welcome to this forum. Changing parameters is only possible via the cursor keys or by software. As far as i know you can only read/write the inputs/outputs of LOGO! with this module. Here are some more infos: http://support.automation.siemens.com/WW/view/en/14291961/133300 https://mall.automation.siemens.com/WW/guest/index.asp?aktprim=0&nodeid=10011668&lang=en&display=t A solution to select different paramters with this module could be: Place more timers (for example) whichare different prametrized and select them by activating virtual inputs with the KNX/EIB module. Regards Fux |
2/17/2007 5:17 PM | |
Posts: 2 Rating:
|
Thanks Fux "Changing parameters is only possible via the cursor keys or by software" Any other software except SoftComfort? |
Follow us on