5/21/2012 9:24 AM | |
Posts: 153 Rating:
|
Hi,all. I have a question. What measuring error can be at connection of the sensor of temperature (2 wires) to the module at length of 5 meters? |
5/21/2012 10:03 AM | |
Posts: 2930 Rating:
|
Hi, here is the link to the actual LOGO! Manual: http://support.automation.siemens.com/WW/view/en/50074616 Listed is: Error limits: 0 .. +200°C +/- 2°C -50 .. 0°C +/- 3°C of final measured value Hope this helps |
This contribution was helpful to
1 thankful Users |
Follow us on