3/23/2007 8:36 AM | |
Joined: 10/18/2006 Last visit: 7/29/2024 Posts: 163 Rating: (3) |
Hi folks, I'm working with a PCS7 project (v6.1 SP1) and I have a short question regarding Asset Management. Where and how could the next specifications be added ?? - Tag - Description - Message - Device Type - Manufacturer - Order Number - Serial Number - Install Date - HW-Revision - SW-Revision These are displayed when opening the diagnostics screen of any component, f.i. the ones shown in the attached files (printscreens). The trouble is that we are not able to find any of them, even the ones that are already displayed (like Tag, Device Type, Order Number…) Where do they come from ? Thank you very much in advance for your help,
AttachmentAsset.zip (492 Downloads) |
3/26/2007 12:03 PM | |
Posts: 1776 Rating: (95)
|
Hi, the information can be found in chapter 1.3.4 in the following document http://support.automation.siemens.com/WW/view/de/21401666 best regards |
3/29/2007 8:41 AM | |
Joined: 10/18/2006 Last visit: 7/29/2024 Posts: 163 Rating: (3) |
Ok, thanks for the info. Ciao ! |
Follow us on