9/28/2013 2:01 AM | |
Posts: 2930 Rating:
|
Hi, if the programming cable is connected and poer goes ON, then LOGO! change to PC --> LOGO! Mode independant if LOGO! was in RUN before Poer off. This is written in LOGO! Manual for 0BA1 PAGE 119. --> disconnect the cable and switch power ON. To chan ge to RUN an the display shows PC --> LOGO! just press cursor down to START. To switch LOGO! back to transfer mode you have to press 3 button at the same time. The 3 Buttons are: C-left, C-right and OK. See LOGO! Maunal for 0BA1 Page 32 or pdf 40. The manual you can download here Scroll down and on the right hand down select "technical dokumentation" Hope this helps Hope this helps |
9/28/2013 6:46 AM | |
Posts: 50 Rating:
|
Thanks Marcjan your solution is right
|
9/28/2013 7:05 AM | |
Posts: 50 Rating:
|
Ohhh This FAQ write in siemens support website in same day i ask about this question
|
Follow us on