7/18/2007 3:23 PM | |
Posts: 10 Rating:
|
Within the current product range of the Logo! there is no seperate HMI. The TP177 Micro is for the S7-200 range of PLC. |
7/18/2007 4:24 PM | |
Posts: 26 Rating:
|
Estimated friend "jonask": In my opinion you must use the standard KNX/ EIB module to SIEMENS LOGO! and late you can connect all the element for this standard, tactil panels, weather station, etc. Standard KNX/EIB it is an international ( allthe important trademarks made productscompatible with this standar ABB, Theben, etc)standar to domotic house or public applications, you can know more about it in the web page(www.eiba.de). I tyhing that it is perfect solution of the problem do you want to resolve, and to teh apllication do you want to make. I have a lot of experience with this standar , if you want I can help you. Best Regards. |
8/1/2007 1:41 PM | |
Joined: 9/29/2005 Last visit: 4/26/2022 Posts: 313 Rating:
|
Hi jonask, as spainlogo already wrote, at the moment you have no chance to use any hmi-device with display for the logo modules except the logo with integrated display itself. of course there is the possibility to use KNX/EIB extension module and add some hmi devices from this list. EIB_HMI_devices If you like them you can find some more information to EIB under following applications: Set8 Set28 But in general i would suggest you to think about if its not too late to switch to s7-200 Any help which fit to your expectations here? best regards Lifrasil |
Follow us on