11/3/2005 8:59 AM | |
Joined: 8/31/2005 Last visit: 10/24/2024 Posts: 217 Rating: (41) |
Hi Reuben! Have a look at this little tool: http://support.automation.siemens.com/WW/view/en/8502062 It says: "ANSWER: You can use the system function SFC64 "TIME_TCK" to generate a random number. From the system time you create the absolute value and then run an integer division with the upper limit as divisor. Determine the remainder left by this division operation. You can use this number as random number." |
Greetings, Chris |
|
Follow us on