3/15/2016 7:24 PM | |
Joined: 3/14/2008 Last visit: 11/1/2024 Posts: 2121 Rating: (949) |
See previous post, forgot the attachment... |
Last edited by: Oreca at: 3/17/2016 9:58:23 AMIf I could help you, you can use the RATE button. Thank you. |
|
3/17/2016 9:48 AM | |
Joined: 3/14/2008 Last visit: 11/1/2024 Posts: 2121 Rating: (949) |
Hi AlwintGru, There are some things you must understand: In the attachment you gave us, is the Compile and download objects screen. Here, you can compile+download all AS programs. For instance, if you have 5 CPU's in your multiproject thus 5 projects, you can compile+download them all at this screen. The option I gave you is to compile+download your chart program on a single CPU. You will compile+download all CFC charts in your current AS program (which are located in your CHART folder). If you have 5 CPU's thus 5 AS projects, you have to do this 5 times. Remark: Since v8.1, there is a option to compile+download selective charts. You only download the changed CFC charts and not the whole program. |
Last edited by: Oreca at: 3/17/2016 9:52:59 AMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
3/17/2016 12:55 PM | |
Joined: 3/14/2008 Last visit: 11/1/2024 Posts: 2121 Rating: (949) |
Hello AlwintGru, OK, nice to hear. Hope everything is clear to you. Let me know what the problem was with the server. If you followed the manual correctly and still problems are present, then I hope Siemens can figure out what it is... |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on