7/1/2019 1:26 PM | |
Joined: 5/7/2018 Last visit: 3/6/2024 Posts: 3 Rating: (0) |
Hello Nzett11 No, didn't get that to work. However when I use the SmartTags function I get get the correct values from my multiplex tags. My code is not done yet. I'm working on autogenerate the memory words that I want to log on my USB. But the logging of the data is working It's a project i'm working on between others project :) This is my code in my test program. Keep in mine that i'm working on automatic generate the memory words on the writing line :) [snip] Attachmentcode.txt (99 Downloads) |
Last edited by: Jen_Moderator at: 07/02/2019 09:09:32Added code as an attachment. |
|
Follow us on