7/11/2020 3:41 PM | |
Joined: 6/20/2020 Last visit: 6/13/2024 Posts: 42 Rating: (0) |
Thanks ixo65, the positive edge solved my problem of excessive counting problem. Scorp, yes i'm using your example and i'm trying an extension for my project. This is for a spraying system : A spray nozzle sprays for a period of time adjustable by the operator. This time is very short. I know the theoretical flow rate of the nozzle. By setting it as a parameter in the LOGO, I want to display the consumption of a cycle (in milliliters) and the total consumption (in liters) Example: Nozzle flow: 4.8l / min Cycle time: 5 seconds First cycle : Cycle consumption: 400ml Total consumption: 0L (0.4L in reality if possible) second cycle : Cycle consumption: 400ml Total consumption: 0L (0.8L in reality if possible) Third cycle : Cycle consumption: 400ml Total consumption: 1L (1.2L in reality if possible) the result is almost good but I always have a problem when launching a new cycle because the reset is bad, the subtraction does not take place I think because it is on the same LOGO cycle as the addition Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/13/2020 07:36:30New subject after splitting |
|
Follow us on