1/5/2022 11:07 PM | |
Joined: 7/28/2021 Last visit: 9/23/2022 Posts: 7 Rating: (1) |
Can always make your own, here is a svghmi button that I made. Change the file extension from .txt to .svghmi and then place it into the following folder: C:\Program Files\SIEMENS\Automation\Portal V17\Data\Hmi\SvgControls\IndustryGraphicLibrary It will show up in Toolbox > Dynamic widgets (hit refresh if it doesn't show up). AttachmentBasicButton.txt (971 Downloads) |
This contribution was helpful to4 thankful Users |
Follow us on