10/18/2023 11:31 AM | |
Joined: 7/19/2022 Last visit: 10/30/2024 Posts: 413 Rating: (70) |
Hello U_cd34e2f3-5a39-4..., Do you have the SIMITIC NET software installed? |
If this Information really helps, you could use the Rate function |
|
10/18/2023 11:56 AM | |
Joined: 10/18/2023 Last visit: 10/19/2023 Posts: 6 Rating: (0) |
Not yet. I will install it now. After installing it, what do I do with it, or can I just use win cc7.4? |
10/18/2023 12:37 PM | |
Joined: 10/18/2023 Last visit: 10/19/2023 Posts: 6 Rating: (0) |
I tried, but it still doesn't change. I installed SIMATIC_NET_PC_V17 cho win cc 7.4 |
10/18/2023 12:45 PM | |
Joined: 7/19/2022 Last visit: 10/30/2024 Posts: 413 Rating: (70) |
I am afraid that the SIMATIC NET V17 version is not compatible with WinCC V7.4 as you can see in the attached compatibility Excel. You must install SIMATIC NET V14 SP1 AttachmentWinCC_V7.4_compatibility-list_es_2023-09-20.zip (273 Downloads) |
If this Information really helps, you could use the Rate function |
|
10/19/2023 5:15 AM | |
Joined: 9/3/2008 Last visit: 10/30/2024 Posts: 928 Rating: (163)
|
Hi, What do you mean "Wincc has problems when I initialize a new project"? Best regards Michael |
Michael |
|
Follow us on