2/29/2024 7:58 AM | |
Joined: 1/17/2019 Last visit: 8/19/2024 Posts: 42 Rating: (5) |
Hello I too experience a similar meaninglessness. I couldn't understand whether the problem was in the computer or the router. What can I do to solve this? I can access the plc program online. wincc communication works smoothly. I can install programs. But I don't see anything in the accessible devices section or proneta. The computer is connected to a wifi network with an access point. Beyond this wifi network, I am talking about communication with the plc, which is connected to a client wifi device. Firewall is off, no antivirus program. everything is clear. What do you think can be done? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 02/29/2024 09:06:53New subject after splitting and text formatting optimized |
|
2/29/2024 10:07 AM | |
Joined: 5/12/2006 Last visit: 10/1/2024 Posts: 22385 Rating: (3015)
|
maybe the used route do not suppport layer 2 broadcasts wg´hich is used for accessible devices searcg |
Follow us on