5/13/2024 10:42 AM | |
Joined: 6/30/2023 Last visit: 10/26/2024 Posts: 7 Rating: (0) |
After installing start drive for V19 TIA V19 shows error TIA Portal can't be started because the installed products of tia portal have different versions. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/13/2024 12:15:51New subject after splitting |
|
5/13/2024 10:51 AM | |
Joined: 1/21/2013 Last visit: 10/28/2024 Posts: 3218 Rating: (499) |
Hi, Please refer to the Sales and delivery release for SINAMICS Startdrive V19 SP1: When using Startdrive as optional package for STEP 7, the installation of STEP 7 V19 Update 2 (109925643) is a prerequisite for Startdrive V19 SP1 Kind regards |
This contribution was helpful to2 thankful Users |
5/13/2024 11:11 AM | |
Joined: 6/30/2023 Last visit: 10/26/2024 Posts: 7 Rating: (0) |
So, I need to install this update 2 for start drive sp1? |
Follow us on