8/4/2016 1:27 AM | |
Posts: 5 Rating: (0) |
Hi, I am running into trouble, I'm quite new to PLC programming, I have only done process control in C langauge.. My project is as follows: 3 vessels / tanks needs to be filled with and amount of water 0-300Ltr only one tank must be filled at a time My input is a waterflow sensor which gives 1 ping per 1 Ltr. All of this works ok.. I think.. Maybe not the smartes way to do it but it seems to work, My problem is: How do get to skip filling tanks if my counter is set to zero in my TDE hmi ?? Any good ideas ? Attached file is my current program..
AttachmentFillingcontrol.zip (170 Downloads) |
Last edited by: Martin_pedersen_fl at: 8/4/2016 1:29:31 AM |
|
8/4/2016 1:29 AM | |
Posts: 5 Rating: (0) |
|
8/4/2016 1:30 AM | |
Posts: 5 Rating: (0) |
|
8/4/2016 7:20 AM | |
Joined: 12/18/2014 Last visit: 9/30/2024 Posts: 33855 Rating: (4210)
|
Here a possible suggestion. The value entered by TDE setpoint is checked for a permissible range (0-300). AttachmentEnabeling_filling.zip (171 Downloads) |
8/4/2016 10:01 AM | |
Joined: 12/18/2014 Last visit: 9/30/2024 Posts: 33855 Rating: (4210)
|
Here is another extended program with control of the pump and transferring the set point in the switch-off of the counter.
AttachmentEnabeling_filling_V2.zip (164 Downloads) |
8/6/2016 9:09 AM | |
Posts: 124 Rating: (13) |
Hello Martin, Here another suggestion. I have considered manual filling mode, but it can be applied in your project. The filled water can be seen in TDE and basic module. If you don't already have a drain water measurement, the values remain even if a drain occurs. For instance, the counters values need to be reset manually (mathematic and analog trigger resets with counter reset automatically). In the future you can use a flow meter to substract values in the mathematic instructions. Regards AttachmentFillingcontrol V3 05 08 2016.zip (166 Downloads) |
Last edited by: Dinos at: 8/6/2016 9:10:13 AMLast edited by: Dinos at: 8/6/2016 9:54:49 AM |
|
Follow us on