11/10/2022 3:53 PM | |
Joined: 9/14/2022 Last visit: 11/18/2022 Posts: 6 Rating: (0) |
Thank you sir, This has pointed me in the right direction. I have one last question if you are able to answer. My question is do you know of a way for the user to be able to change the time in which the timer starts at. For example, I want the user to be able to start the timer at 10 seconds then start counting from there and be able to change where the counter starts every time. I want them to be able to do this without going into the program and use external buttons. Hope this was clear, Cheers.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/11/2022 06:55:48New subject after splitting |
|
11/10/2022 4:29 PM | |
Joined: 9/14/2022 Last visit: 11/18/2022 Posts: 6 Rating: (0) |
By using the up and down keys on the LOGO TD. Thanks |
11/10/2022 4:48 PM | |
Joined: 12/18/2014 Last visit: 7/20/2024 Posts: 33379 Rating: (4143)
|
There is no difference between cursor keys on LOGO! or TDE, for the program is it equal. Need you a example? |
11/10/2022 6:51 PM | |
Joined: 12/18/2014 Last visit: 7/20/2024 Posts: 33379 Rating: (4143)
|
Here's version 2 ...
AttachmentOn-Delay_timer_with_pause_function_0BA8.Standard_V2.zip (640 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on