4/9/2019 10:10 AM | |
Joined: 12/18/2014 Last visit: 10/1/2024 Posts: 33857 Rating: (4210)
|
The LOGO! knows no script processing. The LOGO! knows as programming language only LAD and FBD. |
4/9/2019 10:49 AM | |
Posts: 9 Rating: (0) |
the equation can be simplyfied to 72,43*sqrt(P1-P2) |
4/9/2019 11:58 AM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (207) |
The simplifying is the answer to the constants, the whole pressure range is also okay, but which pressure range would be the normal working area and which accuracy do you need at least ? Regards, Scorp P.S. See attached example program, how to calculate SQRT in the Logo. This is done with the inverse function by searching for a value x, where x^2=P1-P2. You need to scale the amplifiers for the pressure and the result depend on the required units. AttachmentSQRT1.zip (199 Downloads) |
Last edited by: Scorp at: 4/9/2019 1:24:17 PM |
|
4/9/2019 5:50 PM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (207) |
Check for actual Logosoft version 8.2, make an update, if not. SQRT1 is with activated Logo 8 FS4, in next attached file i have saved the same program for Logo 8 Standard, try this for test. Regards, Scorp AttachmentSQRT1 Logo8.0.lsc.zip (189 Downloads) |
4/10/2019 8:55 AM | |
Posts: 9 Rating: (0) |
still cant open it but i only have demo version on this computer so i will try on another later today |
4/10/2019 7:01 PM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (207) |
Which version do you have exactly ? Normally it doesn't matter to have demo or full version, only transfer from and to Logo is deactivated as i know. If you have an older demo version, then download the available demo version 8.0. The newest full version is 8.2 Regards, Scorp P.S. attached a PDF version for manually creation of the program AttachmentSQRT1.pdf (185 Downloads) |
Last edited by: Scorp at: 4/10/2019 7:15:22 PM |
|
Follow us on