10/15/2017 8:33 PM | |
Joined: 9/2/2013 Last visit: 11/6/2020 Posts: 48 Rating: (19) |
Hi, here are IOT2000 boards support and libraries for Arduino IDE: https://github.com/sblyolcubal/arduino-iot2000 Installation instructions and descriptions are on the GitHub page. Differences to Intel i586 boards support: - Serial3 (X30), Serial4 (X31) and SerialUsb (USB X60) support If you found any errors, please open an Issue on GitHub. Any suggestions and ideas for are welcome. |
This contribution was helpful to1 thankful Users |
10/23/2017 6:46 PM | |
Joined: 9/2/2013 Last visit: 11/6/2020 Posts: 48 Rating: (19) |
In new version added: Upload sketch via LAN. |
This contribution was helpful to1 thankful Users |
11/16/2018 5:12 PM | |
Joined: 2/19/2007 Last visit: 8/14/2024 Posts: 10 Rating: (0) |
Hi Ocean i tried to download from the link https://github.com/sblyolcubal/arduino-iot2000 but it seems it is no longer present on GitHub. I am trying to port a sketch from an Arduino Zero and the known issue of the udp remoteip and remoport is frustrating. I do not know if the above libraries fixed this and other bugs too but I really hope so. I do not understand why Siemens keeps on declaring this is compatible with the Arduino and then they do not give developpers a serious and professional support. There are plenty of projects and ideas ready to be ported in a professional and industrial enviroment and the IOT20x0 may be the solution but with this kind of support they will remain in the drawer. Think also about the promise to have libraries for profinet usable by the Arduino Ide. As far as I know there is nothing yet... it is a pity. regards and thank for any help from you or other experts. |
11/16/2018 10:17 PM | |
Joined: 9/2/2013 Last visit: 11/6/2020 Posts: 48 Rating: (19) |
Hi pippo, the IOT2000 board support for Arduino IDE is written by a other person and not from me. I write this person and ask why they delete the IOT2000 Library. They answer me, that the IOT2000 board support is forked from Intel Galileo board support https://github.com/01org/corelibs-galileo and have problems with intel license clarification. Therefore this person deletes the IOT2000 Library from GitHub. If you need support please write your problem here. Best regards Ocean |
Follow us on