5/30/2016 12:34 PM | |
Posts: 1 Rating: (0) |
Hi, I am so badly looking for 6 digit address area solution. Is it possible to get MBMAREQ source to make my own solution ? thanks Marko |
7/13/2016 4:31 PM | |
Posts: 1 Rating: (0) |
Dear TIBI68, First I would like to thank You for creating this driver. I have a problem in communicating cp341 with koyo click as a test connection. I have taken the all steps provided in the manual and still i cannot read or write to dedicated registers. The parameters for koyo click is setup as the same as the cp 341. The Tx led is pulsing with ~0.5 Hz but the Rx led does not blink - CP side On the koyo side both leds are blinking. I have tried to switch the wires and still i cannot write or read the registers. the koyo click addressing of the registers are: 400005 for writing and 400003 for reading. i have called the MBMAREQ with the address of registers with one zero less. I am hopeful that You can take Your time to look at my problem. Best regards, Aleksandar |
7/19/2016 11:15 AM | |
Posts: 1 Rating: (0) |
Hi TIBI68, I want to use your MBMA 340 code to read coils and registers from deepsea 5510. I have connected the cp 340 to that controller and after downloading the program and changing communication parameters in the cp 340, I am able to see TX and RX Blinking .The only challenge i have is how i can read data from the deepsea slave. I have attached part of deepsea registers and i just want you to help me how i could read some thing for example battery voltage which is at register 1029 in the manual. Regards, Willey Attachmentaddress.pdf (633 Downloads) |
Last edited by: willey at: 7/19/2016 2:20:24 PM |
|
7/30/2016 9:12 PM | |
Joined: 5/12/2011 Last visit: 8/21/2024 Posts: 78 Rating: (1) |
Shall i use this sample backup for Estabilishing communication S7 - 315 & EM6430 Energey meter which is supporting Modbus RTU communication using CP 341 card. |
8/2/2016 9:11 PM | |
Joined: 9/2/2012 Last visit: 8/15/2024 Posts: 711 Rating: (30) |
Dear TIBI68,
I didn't check the sample project with the hardware. But i would like to say "THANK YOU" for your effort and attention to the feedback. Also for sharing your "hard-work" for free . Really Gr8 Job .. You deserve more than 5* |
|
|
This contribution was helpful to2 thankful Users |
Follow us on