3/20/2020 4:51 PM | |
Posts: 19 Rating: (1) |
Hello, I recap the principle of runing of cylinders. Please, se the document in appendix. I1 is the signal which is on when both hand are pushing the button, so comparing to before, now I have only one signal for both hand. Please, I have two demand now: 1) to adapt the previous program that I use I1 for both hands, and I6 for start blowing. 2) to explain me why or how to load on logo! because your previous program I didn't been able to load on logo! Thank you in advance. AttachmentPrinciple of programe.pdf (232 Downloads) |
3/20/2020 10:43 PM | |
Posts: 19 Rating: (1) |
Hello, yes , you are right. thank you |
3/20/2020 10:48 PM | |
Posts: 19 Rating: (1) |
Hello, to 1), the I6 switch the output Q2 to start blowing air. to 2), I saw during manipulation that shown also the FS4. thank you 😊 |
3/22/2020 6:04 AM | |
Joined: 12/18/2014 Last visit: 9/30/2024 Posts: 33855 Rating: (4210)
|
I hope now it is so as you want....
AttachmentTwo_cylinders_FS4.zip (227 Downloads) |
This contribution was helpful to1 thankful Users |
3/22/2020 6:50 PM | |
Joined: 12/30/2018 Last visit: 9/28/2024 Posts: 3 Rating: (0) |
krijg fout melding bij open van laatste programma van 22-03-2020 |
Follow us on