1/30/2024 7:49 AM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, finally we released a realtime image (based on Example Image V1.3.1) including the PNDriver for the IOT2050. Everything you need can be found on the download page. There the so-called "test_app" is included, which allows you to manually read and write data from PN devices - see IOT2050_RT_PN_Driver_Quick_Start.pdf We are currently working another example with 4 use cases you can also use a base for own developments. When it comes to questions regarding programming, API, etc. please see the documentation in IOT2050_RT_PNDriver.zip and if further support is required please see this website. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to4 thankful Users |
2/12/2024 5:41 PM | |
Joined: 2/18/2021 Last visit: 8/23/2024 Posts: 8 Rating: (0) |
Hi bergmanu, we're trying to get this running with IM 155-6 PN ST. We fail on your 4th step with the application example (set the PN driver to mode "operate"). The status LEDs of the distribuited IO don't stop blinking but the error LED is turning red/on. Please find the attached screenshots. Do you see any error/mistake? Unfortunately the online diagnosis of the ET200SP says everything's fine when the error LED turns on; test_app seems to be stuck on that step and doesn't come back to the menu. Thank you, Dominik AttachmentIOT2050-ET200SP.pdf (316 Downloads) |
2/12/2024 5:44 PM | |
Joined: 2/18/2021 Last visit: 8/23/2024 Posts: 8 Rating: (0) |
Forgot to attach the console output of step 4 (turning operation mode on). |
2/23/2024 12:32 PM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, can you check the distributed IO with Proneta? Proneta usually gives more helpful diagnostic data Is the IM's error LED on or the ones of one or all modules? Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on