6/2/2020 1:12 PM | |
Joined: 5/31/2011 Last visit: 8/6/2024 Posts: 190 Rating: (31) |
EDIT: Scroll down to later post for correct answers! Hey all, We want to test if we can get a S7-1200 CPU send data to Microsoft Azure IOT-Hub (MQTT). Link to Siemens docs: FB "LMQTT_Client" for Simatic S7-1200/S7-1500" I'm using TIA-Portal V16 upd1 and a CPU1214C V4.4 (6ES7 214-1HG40-0XB0) At this point I'm not getting close in to having a connection with the IOT-Hub. So any help or explanation is helpfull. Maybe it's not possible with Azure and should I try Amazon's IOT-Hub (if that is possible). I'm not sure what to insert concerning the Siemens Function block:
So anyone got it working? Maybe a post an example? PS: I have never done a thing like this. The tutorials on Azure are all in other programming languages then SCL, so that's not making life easier for me. The "certificates" thing is a pain. I have created a certificate with OpenSSL, but don't know the steps in Azure to validate or take ownership or whatever I need to do to get it working. Thank you in advance |
Last edited by: ThaKibosh at: 06/02/2020 13:12:56Last edited by: Jen_Moderator at: 06/03/2020 07:15:50Optimized link. Last edited by: ThaKibosh at: 06/05/2020 08:11:25Last edited by: ThaKibosh at: 06/02/2021 11:17:12 |
|
6/4/2020 10:03 AM | |
Joined: 4/25/2017 Last visit: 9/24/2024 Posts: 430 Rating: (66) |
Hi, There is an example for connecting CC7 to Azure cloud. I think it will help you for connecting MQTT_FB Configuring of the CloudConnect 7 with MindSphere, Microsoft Azure and Amazon Web Services (AWS) |
Best Regards, |
|
1/5/2021 12:49 PM | |
Posts: 2 Rating: (0) |
could you please explain how you got it working ? regards |
3/14/2021 5:07 PM | |
Posts: 2 Rating: (0) |
for you last post do you need a CP module with a 1200 ? regards |
Follow us on