9/25/2021 5:04 PM | |
Joined: 1/6/2018 Last visit: 9/16/2023 Posts: 52 Rating: (1) |
2 even simpler versions, one with time measurments and one with lessons learned from time measurmens but applied with sensors. Can anyone look at the pwm circuit and tell me if I have applied it well, please? AttachmentD2.zip (459 Downloads) |
Last edited by: atsimas at: 09/25/2021 17:09:39Last edited by: atsimas at: 09/26/2021 07:07:33 |
|
9/3/2022 9:45 PM | |
Joined: 1/6/2018 Last visit: 9/16/2023 Posts: 52 Rating: (1) |
This is an updated version of the before program with items readdressed and simplified. You are one could suppose, the limit switch of the shutter. This shutter has 3 sensors at 3 positions. I1 top position of shutter, I2 middle position of shutter, I3 is low position. I4 Auto/Manual is on for auto. Based on the 1st (circulator) temperature you need to act. You must progressivelly lower or raise the shutter based on the temperature. (celcius *0.1) Areas are 0-540 (as 54 c), 600-700, 750-1500. you shouldn't jump from 1st to 3rd positions, As this will create conflict, probably, (more testing is needed for when not working normally I suppose) thus, Malfunction will manifest and I think a screen should pop out also, I am not sure if this works, presently. I6 reset will be needed. I7 and I8 is manual Auto / Manual should be off to avoid conflicts.. I have conviniently put illustrations to see, when program asks for what. Search for the red letters. Total time for actions is max 14 seconds, or else I6 is needed as well high temperatures etc etc. Please point me to everything you think can be done better or if I am missing sth etc etc. Obviously I myshelf did. So.. AttachmentΗλιακός V4fina ++l with sensors.zip (428 Downloads) |
Last edited by: atsimas at: 09/17/2022 07:52:58Last edited by: atsimas at: 09/17/2022 17:33:02Last edited by: atsimas at: 09/17/2022 17:48:47Last edited by: atsimas at: 09/17/2022 18:41:04 |
|
Follow us on