1/19/2021 1:18 PM | |
Posts: 14 Rating: (0) |
I downloaded this exact document as well, but couldn't figure out how to transfer that to the machine. I used a USB stick first then a card reader using the device update tool with this file: SIMOTION_FWSP_V4_3_SP1_HF23.zip But I don't know how to transfer this d4xx_v43sp1hf23_s120_v26sp2hf19.zip file to the device. Do I simply copy the files to the CF card or do something else? I downloaded the fw file that you specified, installed the fw support package first, copied the fw files into the installed fw support package then used the device update tool in scout again to transfer the fw file to my CF card and the version seems to be ok now. The RDY led is constantly green and STOP led is constantly yellow since the device is in stop mode. All other LEDs are off now. The version name on the CF card is also correct. (Not D445-2 at least) So the version problem should be fine now. But I still have the same exact problem with the same exact error code. (ret = 0xbe0b0028) What else should I do? |
Last edited by: turk.mehmetcan at: 01/19/2021 14:48:58 |
|
This contribution was helpful to1 thankful Users |
Follow us on