1/17/2019 3:38 AM | |
Posts: 1283 Rating: (105) |
Hello All, Is there any readily made VFD available for Single Phase In and Out 230V AC? thanks, Jay |
1/17/2019 10:23 PM | |
Joined: 9/27/2006 Last visit: 10/21/2024 Posts: 12290 Rating: (2688) |
Hello guys; Siemens did provide some Micromaster 420 drives with 1-phase input for 3-phase motors. But drives for 1-phase motors are more difficult to find on the market. Here is one option: https://www.wolfautomation.com/blog/leesons-single-phase-unicorn/ There might be more on the web... Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
1/18/2019 1:09 PM | |
Posts: 1283 Rating: (105) |
#dP is right. I am looking VFD for Single phase Motors. @dchartier I did find the same link while searching online. But reluctant to go further with that. Because of this less common VFD for Single phase motor, I am in doubt whether these VFD available will be really able to fit the motor or it will burn out the Motor coils. So just put it here to see whether there is anyone out here worked with this kind of VFD. My thoughts after going around online is that, it is not really good to have a VFD for Single phase Motor. Three phase Motor is the best and you can play with VFD for this kind without any worries. So kinda gave up the search. Thanks for all your responses though.
|
Follow us on