2/26/2024 2:22 PM | |
Joined: 3/30/2020 Last visit: 6/1/2024 Posts: 4555 Rating: (950) |
Your problem is not related to the BCD representation. It would be beneficial for you to have a look how the S5TIME type is constructed. The documentation provided with the software is complete in this regard. But you may have a look at: [LINK: Storing the S5TIME data type]. It may be worth considering the use of an IEC Timer instead. These are available in the library of instructions. [LINK: How do you measure the time in STEP 7 V5.x?] -- look at example 2. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on