3/26/2018 3:51 PM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating: (71)
|
Yes that's normal. The reader doesn't need to be projected. It only appears in TIA selection tool. To configure the reader you need to install PCT (Port Configuration Tool). You can then open PCT from HW-Config of the CM. This might also help you: |
3/27/2018 8:46 AM | |
Joined: 3/26/2018 Last visit: 5/30/2024 Posts: 38 Rating: (1) |
Thanks! I understand what you are saying, but can I also configure it without the S7-PCT?(see attachment) |
3/28/2018 11:22 AM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating: (71)
|
Nope, you'll need the PCT: You'll also need a IODD file for the RF240R to import it into PCT: I suggest you to follow the description from the application example to configure the hardware. |
4/10/2018 9:26 AM | |
Joined: 3/26/2018 Last visit: 5/30/2024 Posts: 38 Rating: (1) |
Thank you very much! I'll figure it out and if something won't work, I'll let you know! |
4/10/2018 7:04 PM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating: (71)
|
If your IO-Link master has the newest firmware (V2.2) you'll need to install PCT 3.5. But the update is for free so why hesitate to install the newest version? |
Last edited by: Owei at: 4/10/2018 7:06:20 PM |
|
4/11/2018 8:35 AM | |
Joined: 3/26/2018 Last visit: 5/30/2024 Posts: 38 Rating: (1) |
|
4/11/2018 9:04 AM | |
Joined: 3/26/2018 Last visit: 5/30/2024 Posts: 38 Rating: (1) |
It Worked, restarted the VM! so I only need to install IODD now and than it should work perfectly ? |
Follow us on