9/13/2021 4:13 PM | |
Joined: 12/12/2016 Last visit: 7/25/2025 Posts: 640 Rating:
|
Hello, Yes, you can collect data from the S7-300 over S7-Communication -> Check out this example. To make the data available over OPC UA, it is possible to use the OPC UA Client nodes in node-red to write this data onto an OPC UA Server (example). If you want to use the OPC UA Server Nodes directly in Node-Red, I would recommend switching to an IOT2050 as these nodes do not run stable on the IOT2040 and will crash after a few hours of use. But there are of course other implementations of OPC UA Servers that can be used on the IOT2040, e.g Open62541. BR |
Follow us on