8/16/2020 10:41 AM | |
Posts: 1 Rating:
|
Hello, I am using Siemens 840 d controller I am getting the following error every day when I try to reference the machine in X direction 20005: AXIS X1 reference point approach aborted After resetting the alarm, the machine again starts referencing for few seconds and then gives either (25201) ATC drive fault or X1 drive fault. To clear the drive fault errors I have to restart the machine and do the same procedure as above for almost 7-8 times until the machine gets into the reference position. So, can you please help with the error? ------------------------------------------------------------------------------------------ |
Last edited by: SP_41 at: 08/16/2020 10:42:21Last edited by: Jen_Moderator at: 08/17/2020 06:23:50New subject after splitting |
|
8/17/2020 6:35 AM | |
Joined: 10/17/2007 Last visit: 7/14/2024 Posts: 4008 Rating:
|
please post one picture when the 1st time machine has 20005: AXIS X1 reference point approach aborted--making screen-shot in the "Diagnosis" to see all alarm, I think there may have other alarms Do you ever check manual by yourself, there is alarm explanation for 20005 or 25201 in the manual "840D Diagnosis Manual", Google it and
|
If you like my comments please |
|
Follow us on