3/13/2025 12:18 PM | |
Joined: 2/17/2016 Last visit: 3/13/2025 Posts: 1 Rating:
|
Why a CPU 1512SP-1 PN has to MAC-addresses? There is only one ethernet port, extendable to 3 ports with a bus adapter, but in that case, the 3 ports have the same IP-address. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 03/13/2025 12:59:41New subject after splitting |
|
3/13/2025 1:22 PM | |
Joined: 1/21/2013 Last visit: 9/19/2025 Posts: 4114 Rating:
|
Hi, As you can see from the equipment manual, your CPU has 4 MAC addresses in use. This is because for a PROFINET device, each interface (X1 for your CPU) has a MAC address and each port has an additional address. Kind regards |
Follow us on