9/19/2021 9:22 PM | |
Joined: 11/9/2014 Last visit: 10/20/2021 Posts: 3 Rating:
|
Siemens: can you please load a TIA BASIC sample in addition to the current TIA Professional sample that is on: https://support.industry.siemens.com/cs/document/109779336/connecting-a-s7-1200-s7-1500-to-a-sql-database-?dti=0&lc=en-WW I can open the project, but when I want to look at the OB1 it gives me the error that I need the professional license. PLEASE? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/20/2021 11:57:37New subject after splitting |
|
9/27/2021 10:54 AM | |
Joined: 8/3/2009 Last visit: 9/15/2025 Posts: 16409 Rating:
|
Hello MavTechMav I Opended Example and there is only a S71500 inside. I created a S71200 and copy and Paste the blocks to S71200. Here is the Basic Project. But I have not tested or compiled to see if it works. But it should be only an example. Perhaps it helps bye Murof AttachmentSQL_S7_1200_CODE_V21.zip (478 Downloads) |
If this Information really helps, you could use the Rate function |
|
10/20/2021 6:19 PM | |
Joined: 11/9/2014 Last visit: 10/20/2021 Posts: 3 Rating:
|
Thank you for the suggestion. I have now tried that - lets see if I get an answer :) |
Follow us on