Industry Online Support
Technical Forum
6/6/2012 10:52 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello Experts, On Pegard make 6 axis HBM machine, boremachiningoperation is successfully executed with R parameter part programe (Please find attached here with the sample part programe) Now we would like to machine taper bore. Can anybody guide us as how to use R parameter to machine taper bore? Bore size is max dia 488.28 mm, minimum bore dia 474.8 mm, length is 425 mm. Thanks in advance. DEEP. AttachmentBORE PART PROGRAME.pdf (78 Downloads) |
7/5/2012 4:59 AM | |
Posts: 15 Rating: (0) |
Use the same logic. Instead of hardcoding the axis movements, use R parateters. For example instead of x10 use X=R0 and if R0 has a value of 10, it will move 10.
|
7/5/2012 5:49 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Sorry, I could not get you. Could you write the program & attache it here? |
Follow us on