6/18/2008 7:04 PM | |
Posts: 297 Rating: (41) |
The PCU50 has been cancelled - see http://support.automation.siemens.com/WW/view/en/25907766 The original PCU50.3 did not have any serial ports. Siemens just announced that they will include one serial port on all PCU50.3s - see http://support.automation.siemens.com/WW/view/en/29351390 If you need another you'll need to add a PCI card (Siemens has one) or use a USB to RS232 adapter. Not familiar with the OP-17. There are a range of current operator panels from OP-08 to OP-15 - pick your size. OEM custom screens covers a lot of options. If it is a "wizard" screen, it may still work. Anything else (easymask, transline, pro-tools, wincc, HMI programming) will probably need to be re-done, but you might get lucky. PCU50's run WInXP now and don't officially support 16 bit Windows apps. HTH, SteveA |
3/17/2016 2:16 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by U_7a700288-c1f7-4123-b22c-769636b83abc is split to a separate thread with the subject Sinumerik HMI, can't view the data. Best regards |
8/11/2017 2:11 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (171) |
New question published by augt is split to a separate thread with the subject Need to transfer all those screens from my MMC103 to PCU 50.3.. Best regards |
Follow us on