10/30/2022 7:31 PM | |
Joined: 10/29/2022 Last visit: 11/1/2022 Posts: 5 Rating: (0) |
I just downloaded the demo version of LOGO! Soft Comfort v8.3, and every time I try to save a diagram to disk I get the following error: Exception: java.lang.SecurityException: JCE cannot authenticate the provider BC The logs show the error is caused by Causedby:java.util.jar.JarException:file:/Applications/LOGOComfort_V8.3(Demo)/lib/bcprov-jdk15to18-164.jarhas unsigned entries - org/bouncycastle/LICENSE.class How can I solve this? Thanks! Attachmentsoftconfort_save_exception.txt (569 Downloads) |
10/30/2022 7:36 PM | |
Joined: 12/18/2014 Last visit: 9/12/2024 Posts: 33757 Rating: (4191)
|
Is your Java up to date? |
10/30/2022 7:38 PM | |
Joined: 10/29/2022 Last visit: 11/1/2022 Posts: 5 Rating: (0) |
Java 8 update 351, just installed today |
10/30/2022 7:44 PM | |
Joined: 12/18/2014 Last visit: 9/12/2024 Posts: 33757 Rating: (4191)
|
Then deinstall the demo and try to install it new ... Which OS use you? |
10/30/2022 7:47 PM | |
Joined: 10/29/2022 Last visit: 11/1/2022 Posts: 5 Rating: (0) |
macOS 13, with an M1 processor |
Follow us on