3/30/2022 4:15 PM | |
Joined: 3/29/2022 Last visit: 11/30/2023 Posts: 1 Rating: (0) |
I am getting the same error $ 613 DB-Fehler. I have a S5-95 and a TD10 Display unit. The TD10 was displaying "Ready for Transfer" If you watched it boot up you could see a quick flash saying "Flash Memory Failure". The machine runs fine so I think it was the EPROM in the TD10. I replaced the EPROM in the TD10 and now it displays "$ 613 DB-Fehler". I have reloaded the EPROM on the S5-95 and the machine still works but the TD10 does not. How can I get the S5-95 reload the program to the TD10 or is that not possible? Any chance anyone has a manual for the TD10? Thanks, Steve
------------------------------------------------------------------------------------------ |
Last edited by: SteveMol at: 03/30/2022 19:24:56Last edited by: SteveMol at: 03/30/2022 21:06:49Last edited by: Jen_Moderator at: 03/31/2022 09:36:39New subject after splitting |
|
Follow us on