(0)| 4/11/2022 7:44 PM | |
|
Posts: 5 Rating:
|
Hi, To use the Script debugger in Chrome using WinCC Unified, I have followed this link: Script Debugger with WinCC Unified and this YT-video: https://www.youtube.com/watch?v=GDsmuIXODGU When I restart the project in the Simatic RunTime manager, I only have about one second to press inspect on the target. Which is the startscreen of the project. After that the target disappears. After a screenchange the debugger should be refreshed. When I do that, it seems the debugger is not able to find the target anymore. I have the debugger enabled in RunTime manager. I Hope you can help me. Kind regards |
Last edited by: Jen_Moderator at: 04/19/2022 08:18:05Video embedded. |
|
Follow us on