2/3/2023 10:18 AM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
Hi As from TIA V18 it is possible to configure the decluttering feature for WinCC Unified. The configuration allows the programmer to have precise control of which objects will be visible or not according to the zoom factor, that means the programmer should define rules to it works. Settings:
Sample project AttachmentProject33_20230126_0723.zip (590 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
1 thankful Users |
Follow us on