9/23/2024 8:48 AM | |
Joined: 3/12/2024 Last visit: 10/8/2024 Posts: 50 Rating: (0)
|
Hello, looks like you are using IndOS and not the Example Image from our Download Page. Unfortunately there is no way to run the iot2050setup command in the Industrial OS. I would recommend you to use the Example Image and to have a look in our Serial Connection Example. As you mentioned the switchserialmode is not really persistent, but if you don't want to switch to the Example Image you should be able to call these commands... IOT2050 Basic:
IOT2050 Advanced:
The only problem is that you need to call these commands with every reboot so you should add this command to an autostart-script. BR |
Follow us on