(0)| 2/26/2025 9:24 AM | |
|
Joined: 1/21/2013 Last visit: 1/15/2026 Posts: 4400 Rating:
|
Hi D0eber, You should be aware of the two different implementations of the OpenFaceplateInPopup method. There is one in the UI scope and another in the FaceplateType scope. Within a faceplate type, you cannot assign interface data that is not needed because it is inherited by the opened faceplate from the base faceplate. This is likely the cause of the error. Kind regards |
| 2/26/2025 10:42 AM | |
|
Joined: 1/21/2013 Last visit: 1/15/2026 Posts: 4400 Rating:
|
Hi D0eber, Unfortunately, not all entries in the trace log are useful, so you may want to ignore them. However, if you provide some more detailed information about your system and device, it may be reproducible or already known to someone in the community. You can also create a support request. Kind regards |
Follow us on