(1)| 3/4/2025 10:39 AM | |
|
Joined: 8/3/2009 Last visit: 1/21/2026 Posts: 16653 Rating:
|
Hello alberrdz I think its not that easy to just put them into the common archiving folder. This way is for liking backup segments if used. But you have to care about deleteing them again after usage because every additional linked segment increses the performance load to the system. also the segments has to be from the same project (same configuration and tag management...). If it works -> OK thats perfect for you but you should delete the data again after you do not need it. If you want to integrate the segments into the running taglogging you can have a look at this FAQ: https://support.industry.siemens.com/cs/ww/en/view/24193864 Its for WinCC V7/8 but works the same way in WinCC Professional. If the new project is the same as the old one but only without databases then this way could be a better solution Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on