2/12/2015 12:42 PM | |
Joined: 6/22/2013 Last visit: 11/24/2023 Posts: 141 Rating:
|
Good morning to all I have problem installing Tia V13 SP1, the finalaizar installation gives me an X is an error, and ended that occurred after two hours or so, the virus can disrupt the installation, when being installed, virus detected several times, and he said he was moved to trunk. But supposedly SP1 was installed on my laptop but it opened the antivirus off, but can not communicate with PLCSIM gives me fails. Deputy lp that left me in notepad, fails. Greetings.
AttachmentFalla Instalacion Tia V13SP1.docx (365 Downloads) |
3/22/2015 3:09 PM | |
Joined: 9/9/2011 Last visit: 2/25/2025 Posts: 102 Rating:
|
hello same error for me ! I have install only TIA V13 SP1 + Update 1 (I don't want to have PLC SIM) No problem on TIA13 SP1 Update1 working well but problem on WINCC V13 SP1 Update 1 install problem ! During this install, i had not enought battery and computer shutdown.... I try to desintall it with différents program.... or with Windows but problem are same.... http://i62.tinypic.com/6yo1w1.jpg AttachmentSIA_WINCC_PROFESSIONAL_V13_SP1@15-03-22_11-52-32_summary.txt (239 Downloads) |
Last edited by: GB002 at: 3/22/2015 3:12:29 PMLast edited by: GB002 at: 3/22/2015 3:13:37 PMLast edited by: GB002 at: 3/22/2015 3:14:30 PMLast edited by: GB002 at: 3/22/2015 3:15:22 PMLast edited by: GB002 at: 3/22/2015 3:19:55 PM |
|
Follow us on