6/1/2014 11:06 AM | |
Posts: 559 Rating:
|
Dear KIRAN_DABHI, If this is the case then you do not have any chances to work without backup of HMI. If it is not possible to get the backup from supplier then you can do one thing. if TP is working with updating values from CPU the You just go to individual screens into and try to find out the tags for all screens by monitoring the values from CPU. If some supplier provides the machine then they are doing good programming like making separate DB for HMI functions. So in your case also if this is available then you just find out that DB & from there you find the tags. I have already put one post to siemens related to this issue. Please see the below link. |
5/19/2017 9:17 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4760 Rating:
|
New question published by ingesosagt is split to a separate thread with the subject Can't load PSB file to 700 IE V3 panel. Best regards |
Follow us on