12/2/2020 9:04 PM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
Hi, “Simple Samples” are small projects that demonstrate simple features. The target is giving a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. As from the TIA V16, there was the introduction of the WinCC Unified. This is an engineering platform for HMI Comfort Unified and for WinCC Unified PC. It brings many news regarding the WinCC Advanced / WinCC Professional. One of the news of WinCC Unified is the support of List Box This sample project exemplify both elements. TIPs for Check box
Project (archived and ziped) AttachmentTextList.zip (1353 Downloads) |
Last edited by: Denilson Pegaia at: 12/02/2020 21:09:05Last edited by: Denilson Pegaia at: 12/03/2020 02:47:38Last edited by: Denilson Pegaia at: 12/09/2020 11:12:39add select item text/example Denilson Pegaia |
|
This contribution was helpful to
2 thankful Users |
Follow us on